Chart Settings

Specify the trace display settings for the chart.

You cannot select a trace if it is dim. To select the trace, go to Settings > Trace Logging Selection, and select the trace that you want to perform data logging.

Trace

Trace Thickness – Set the trace thickness. This setting is only available for Multiple Traces View.

Focused Trace – This setting is only available when Single Trace View is selected. Select a desired trace to focus and display on top of all the other traces on the chart.

Hide Unfocused Trace – This setting is only available when Single Trace View is selected. Hide or show the other traces in the background. When enabled, only the focused trace is displayed on the chart.

Vertical Scale – Set the scale for the vertical axis (y-axis). Click the drop-down arrow to set your desire scale.

Vertical Offset – Set the offset for the vertical axis (y-axis). Click and edit the offset on the field and click on the unit to change the unit of measurement.

To set the trace color, click the color box and select the desired color from the color palette.

To show or hide the trace(s) display on the chart, select or clear the check box of the trace(s).

Axis

X-Axis Grid Labels – Set the x-axis grid labels. Select from Relative To Zero (default), Date Time in local time, or Date Time (UTC) relative to Universal Time Coordinated time.

See Also

Data Logger Settings

Trace View

Chart Controls

Markers